DIO#.SOURCEID

Description

DIO#.SOURCEID sets the digital I/O source ID, for sources that require an ID.

Examples

Usage

DIO#.SOURCEID can be used to select the compare channel whenDIO#.SOURCE = 4 (Compare).

Code

The following commands set the source of digital IO 1 to compare channel 1, and digital IO 2 to compare channel 2.

--> DIO1.SOURCE 4
--> DIO1.SOURCEID 1
--> DIO2.SOURCE 4
--> DIO2.SOURCEID 2

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare source 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DIO1.SOURCEID

368ah

06h

Unsigned8

-

-

Read/Write

No

DIO2.SOURCEID

368bh

06h

Unsigned8

-

-

Read/Write

No

DIO3.SOURCEID

368ch

06h

Unsigned8

-

-

Read/Write

No

DIO4.SOURCEID

368dh

06h

Unsigned8

-

-

Read/Write

No

DIO5.SOURCEID

368eh

06h

Unsigned8

-

-

Read/Write

No

DIO6.SOURCEID

368fh

06h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DIO1.SOURCEID

22300

571C

Unsigned8

Read/Write

-

DIO2.SOURCEID

22301

571D

Unsigned8

Read/Write

-

DIO3.SOURCEID

22302

571E

Unsigned8

Read/Write

-

DIO4.SOURCEID

22303

571F

Unsigned8

Read/Write

-

DIO5.SOURCEID

22304

5720

Unsigned8

Read/Write

-

DIO6.SOURCEID

22305

5721

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DIO1.SOURCEID

22300

Unsigned8

Read/Write

-

DIO2.SOURCEID

22301

Unsigned8

Read/Write

-

DIO3.SOURCEID

22302

Unsigned8

Read/Write

-

DIO4.SOURCEID

22303

Unsigned8

Read/Write

-

DIO5.SOURCEID

22304

Unsigned8

Read/Write

-

DIO6.SOURCEID

22305

Unsigned8

Read/Write

-